Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Our recent article How to reduce dust by applying the STOP principle explored various measures that support minimizing exposure to dust. Since the 1990s, Hilti has been developing a rich competence in the field of virtually dust-free working.
Hilti has its own Dust Research Center in Germany where all kinds of measurements and analyses take place. Hilti’s own Dust Experts are part of a community actively developing relevant standards like EN 50632. As a result, Hilti has developed a broad range of dust control solutions for the construction industry.
The Hilti Dust Research Center plays a central role in ensuring that Hilti power tools are optimized to control dust. At Hilti this means that dust optimization for tools spans the entire development process, starting already at the design stage.
Just recently the Dust Research Center in Germany has been reviewed by the British Health and Safety Laboratory. It was confirmed that the Hilti test lab meets all rigorous requirements.
Mr. Saunders, who reviewed the Dust Research Center, commented on the Hilti approach to tackle dust: “It’s clear that the design of extraction has not been added to the tool as an afterthought; rather, it has been embedded into the tool design at an early stage.”
But let’s go back to the variety of tasks of our dust researchers. The Dust Research Center has a crucial consultancy function for the development teams which spans all stages of product development. As Hilti offers the whole system chain for dust control (from the insert to the vacuum cleaner), we can optimize each component and interface.
Our dust researchers also apply Computational Fluid Dynamics (CFD) simulation. This is a technology that can predict dust flow profiles within the housing of Hilti tools, which are then prototyped and tested by Hilti. Here’s such a CFD image:
Supporting the product developers with expert knowledge is one part of the job. The dust researchers also measure dust generated from Hilti power tools and analyze the portion of inhalable and respirable dust produced. These measurements are completed according to EN 50632.
EN 50632 is the standard that defines the dust measurement procedures for suppliers of electric motor operated tools. Part one of EN 50632 covers the general test requirements, while parts two and three cover requirements for the dust measurement of particular types of tools.
Remember our busy Dust Experts in the Research Center? They are also represented in a so called standardization committee. This way Hilti can play a proactive role in developing relevant standards that support improved dust control in the industry. Thus, Hilti was actively involved in developing EN 50632.
Using EN 50632 means that the results from different suppliers are comparable. One specification is that filters used for sampling are weighed in controlled humidity conditions using a balance to a precision of 0.01 microgram – a necessary, but expensive investment (Hilti’s gravimetric measuring equipment, for example, costs €11,000). The standard also demands that the tool is used for an hour and the operation is repeated three times, with the average taken of the three dust samples collected.
Have you ever wondered how these measurements are carried out in real life?
Here’s a look at the equipment used in the Dust Research Center to measure dust. Dust collectors for inhalable and respirable dust fractions including filters for a gravimetrical analysis of the collected dust are worn by the Dust Expert on the chest.
Today, all Hilti electric tools for working on concrete have means to connect a vacuum cleaner or specific dust removal systems (also called DRS in the Hilti world). When controlling dust, it is essential that the complete system around hand-held power tool and vacuum cleaner works well together. A harmonized system is one where power tools, drill bits, discs, blades and other accessories are matched to maximize the amount of dust removed at source, which is then collected efficiently by the vacuum cleaner.
At Hilti we interact with our clients more than 250,000 times every day. This means we learn a lot about the professionals who use our tools, their applications and their specific needs. When it comes to dust control Hilti offers not only dust technologies, but also supports employers to train their teams on the danger of dust.
Here’s a look at the four components of the Hilti system:
Consumables design
Power tool design
Hilti Accessories
Hilti Vacuum Cleaners
You can find more information on dust in our previous article How to reduce dust by applying the STOP principle.
We work together with you
Up-to-date information about changes in our work.
Read more
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.
To see account specific prices and content, please choose appropriate account.
Hilti = registered trademark of Hilti Corporation, 9494 Schaan, Liechtenstein © 2009-2016, Right of technical and programme changes reserved, S.E. & O
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.