Update of quantity
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
If you’re building piping applications then it’s vital to bear in mind thermal expansion – particularly for heating applications.
This is because you will need to allow the pipes to expand and to ensure a uniform distribution of how the pipes move.
Thermal expansion depends on a few key factors:
This is usually the change in temperature between the operational temperature of the pipe and the temperature outside. So, for instance for heating applications, the operational temperature would be around 70 °C and the ambient temperature typically 20 °C.
Share
To see account specific prices and content, please choose appropriate account.